4/22/2010 3:40 PM | |
Posts: 7 Rating:
|
Dear Vithani, my request doesn't relate to your question, but I was looking for a thread, such as 'SIMOVERT VC in SLVC' throughout Siemens forum, and then found yours "Right now I am facing problem of alarm A025 i2t Inverter- in master drive VC. We have drive rated 124 Amp. Application is of Exhaust fan and drive is running on SLVC mode" the staff, who projected our plant, chose the wrong encoder (sin/cos type) by a mistake, which is not compatible with Simovert VC! As a result, the actual speed is lower than setpoint! Can you please tell me, how to turn SIMOVERT VC into SLVC mode?! Thanks! There is a parameter set, which is used now Splitted from A025 in Masterdrive VC. AttachmentDrive M1 03_06_08 last.zip (239 Downloads) |
Last edited by: O_Moderator at: 4/23/2010 8:44 AMnew subject after splitting |
|
4/23/2010 8:47 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already discussed in the following thread SIMOVERT VC vector control mode without encoder - SLVC. Best regards O_Moderator |
Follow us on