5/20/2010 3:05 PM | |
Joined: 9/27/2006 Last visit: 9/9/2025 Posts: 12401 Rating:
|
Hello aym_31; Here is a bit of litterature on PDM and HART connectivity. PDM- HART modem: http://support.automation.siemens.com/WW/view/en/13967584 Manual PDM(HART): http://support.automation.siemens.com/WW/view/en/7717170 http://support.automation.siemens.com/WW/view/en/37565982 Manual Sitrans P, HART interface: http://support.automation.siemens.com/WW/view/en/7353802 The usual connection for HART would be a HART modem, as descibed in the first manual (note the English section, even if the title is in German). However, they do show a connection through Profibus-PA, where a Profibus CP could act as a master class 1 (what would the supporting software be?), in the PDM (HART) manuals. Anyway, have a look and come back if you need more information. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/20/2010 3:08 PMLast edited by: dchartier at: 5/20/2010 3:07 PM |
|
Follow us on