3/15/2010 1:07 PM | |
Posts: 3609 Rating:
|
Import of a Technical Question of an User ZDdd wrote: Dear sir, As a novice in using Siemens PLC I found myself a bit unprepared forPID control. The problem I have is a positioning valve that needs to be controled according a setpoint( comes from a panel), and the valve's position should be read as an analog signal ( 4-20 mA). Could you please, send me a simple example of using STEP Control SFB 42? Thanks in advance. Marko. |
3/17/2010 9:50 AM | |
Posts: 3 Rating:
|
Please if anyone could give me an example of using SFB 42 "CONT_S in S7-300, I would be very gratefull. Kind regards, Marko |
7/1/2010 1:54 AM | |
Posts: 2 Rating:
|
I too am requiring some guidance of setting up my first PID loop to control Speed. Any help will be appreciated. Cheers Frozen |
7/3/2010 8:10 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, Look at Where can you find descriptions and examples of PID control with FB 41, FB 42 and FB 43, and SFB 41, SFB 42 and SFB 43? Hope will helps. Best rgeards, Hristo Mihalev |
Follow us on