(1)| 7/14/2010 12:53 PM | |
|
Joined: 9/23/2005 Last visit: 12/29/2025 Posts: 4435 Rating:
|
Hi, This module can read different ranges of PT 100 temperature (settings), however it cover the range from -240.0°C to 1100.0°C. The temperature is read directly as decimal on the correspondent IW. For example 36,5°C is read as 365. There is a documentation avaliable to this module. See http://support.automation.siemens.com/BR/view/en/43346925 |
|
Denilson Pegaia |
|
This contribution was helpful to
|
|
Follow us on