1/3/2010 11:01 PM | |
Joined: 5/4/2009 Last visit: 11/23/2024 Posts: 914 Rating:
|
Dear experts... I want to control an SIMOREG (6RA7018-6DS22-0) single quadrant drive via a potentiometer and a start/stop switch, also I want to view on the PMU the "firing angle". My questions are: what parameters I should set? on which terminals I should connect the potentiometer? on which terminals I should connect the START/STOP switch? Please I need help. Tomy. |
Aim Higher |
|
8/6/2010 1:10 PM | |
Joined: 9/28/2007 Last visit: 8/10/2025 Posts: 246 Rating:
|
Dear see attached file. may it help you. Attachmenttips_76.pdf (459 Downloads) |
Muhammad Munir |
|
8/6/2010 3:34 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
|
Follow us on