8/20/2010 1:49 PM | |
Posts: 39 Rating:
|
how can i program in SCL in Step7? Is it correct that i need a "plug-in" for Step7 to do this? I can only find LADDER, STL and FBD.. I could REALLY use an example i LADDER mode....!!!! (Step7 V5.4 +SP5) Thanks! Splitted from if then else in S7. |
Last edited by: O_Moderator at: 8/20/2010 1:55 PMnew subject after splitting |
|
8/20/2010 2:16 PM | |
Joined: 9/27/2006 Last visit: 9/18/2025 Posts: 12414 Rating:
|
Hello kasper; First about S7-SCL, Siemens, version of IEC61131-3's Structured Text. You will need the S7-SCL add-on to Step 7, or the Step 7 Professional package which includes S7-SCL, along with S7-Graph (Sequential Function Chart language) and the S7 simulator PLCSIM. 6ES7811-1CC05-0YA5 SIMATIC S7, S7-SCL V5.3 FLOATING LICENSE FOR 1 USER E-SW, SW AND DOCU. ON CD, LICENSE KEY ON FD, CLASS A, 5 LANGUAGES (G,E,F,I,S), AS OF STEP 7 V5.3 WIN2000PROF/XPPROF, REFERENCE-HW: S7-300/400, C7 6ES7810-5CC10-0YA5 SIMATIC S7, STEP7 PROF ED2006, FLOATING LICENSE FOR 1 USER, E-SW, SW AND DOCU. ON DVD, LICENSE KEY ON USB STICK , CLASS A, 5 LANGUAGES (GE,EN,FR,IT,SP), EXECUTABLE UNDER WINXPPROF, WIN VISTA ULTIMATE, WIN VISTA BUSINESS REFERENCE-HW: S7-300/400, C7 STEP 7 Professional supports all IEC languages. In addition to the languages recognized by STEP 7 § LAD § FBD § IL The following are also available: § "Sequential Function Chart" § "Structured Text" An offline simulation of programs created with these languages is included. STEP 7 Professional thus replaces the combination of the individual packages STEP 7, S7-GRAPH, S7-SCL and S7-PLCSIM. Now, there are some libraries of progrms already loaded with your Step 7 package, under the tab Examples (when you Open a program). You should have a few there that have the _LAD_ designation that you can study. You could also look at these S7-300 tutorials, they have samples in LAD and even in SCL if you need them.
|
Last edited by: dchartier at: 8/20/2010 2:17 PM |
|
8/23/2010 3:52 PM | |
Posts: 39 Rating:
|
Hello Daniel Thank you very much!! You have been great help many times now!! Good "quality answers"!!!! I believe it is the 6ES7811-1CC05-0YA5 licens i need for this project! Regards Kasper |
Follow us on