10/5/2010 2:36 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Hi, You are trying to set or reset a bit in one of the parameters through acyclic writing. You just have to send 1 or 0 from your plc to that parameter. Regards, Behnam CPU315 <-> S120, How????? |
10/5/2010 3:15 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Leif, This is a CU parameter. You have to address the CU unit while changing the parameter. There is no such a thing as addressable 0 or 1 in the Drive. Another option is to use AND gate (P20030) or ORgate (P20046) from one of the drives and tie the outputto your parameter and you can change the input to the gate through your acyclic writing. Regards, Behnam CPU315 <-> S120, How????? |
10/5/2010 4:10 PM | |
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Leif, I still think you should be able to write 0 or 1 to that parameter through acyclic writing. But anything like addressing a 0 or 1 in sinamics doesn't exist. Regards, Behnam www.sigmaprocess.ca |
Follow us on