10/8/2010 9:13 AM | |
Posts: 14 Rating:
|
Hi Sir Question 1: I have a project ,have two Wincc server ,and have 16 SICAM PAS Server When PAS Server have change ,I will to doSICAM PAS Wizard on the Wincc Server 1 And Wincc Server 1 is ok, I will to use Project Duplicator Wincc Server 1 project to Wincc Server 2. Than Wincc Server 2 will be import all SICAM PAS data again , but show some error message aboutSICAM PAS Wizard on the below: "WinCC Alarm Logging; Error: Changing message (raw data tag): ID 3322" and these 4 message's data on the Wincc Server 1 are different and Wincc Server 2. Question 2 : The sameSituation, SICAM PAS Wizard show the message on the below: "Scripts; Error: Adding a new station. The maximum amount is exceeded" -------------------------------------------------------------------------------------------------------------- So,How can I to solve these questions for mycustomer. thanks you ! Attachmentcsc_hmi_error.zip (512 Downloads) |
Follow us on