3/23/2011 10:50 AM | |
Joined: 12/1/2010 Last visit: 12/3/2012 Posts: 7 Rating:
|
Hello, unfortunately I can't help you with programming such a HMI.SIEMENS offers a free HMI project for SIWAREX U and WinCC flexible (this is a special SIEMENS HMI software), but you can't open this project without the software WinCC flexible. Link to the project: http://support.automation.siemens.com/WW/view/de/28391777 Regards, Maschex |
Last edited by: Maschex at: 3/23/2011 10:51 AM |
|
3/23/2011 12:58 PM | |
Posts: 206 Rating:
|
Hello Ni, if you have a look to the projekt that Maschex suggested you will see that the data of the Siwarex U are all in the DB9. e.g. The actual value of the channel 1 in in dbw12 .... See also the manual http://support.automation.siemens.com/WW/view/en/28392477chapter 8. Regards ABenno |
Follow us on