2/24/2012 9:17 PM | |
Posts: 27 Rating:
|
dear all, ı want to connect a pac 3100 to pc, which sofware ı need ? also what kind of connection do ı need to ?
|
2/27/2012 10:45 AM | |
Posts: 50 Rating:
|
Hello, The SENTRON PAC3100 has a integrated serial MODBUS RTU interface. You can use the lucky-free software SENTRON powerconfig. Here can you find the actually software for download: http://support.automation.siemens.com/WW/view/en/57887187 Please note: You need a attional usb-RS485 converter for the pc interface. Here a detailed description for the software connecton. http://support.automation.siemens.com/WW/view/en/48014985 For a real powermonitoring software, you can use the SENTRON powermanger software: http://support.automation.siemens.com/WW/view/en/35384803/133200 Attachment05_pi_powermanager_EN_2913.pdf (480 Downloads) |
Follow us on