(0)| 2/22/2007 3:10 PM | |
|
Joined: 8/31/2005 Last visit: 12/15/2025 Posts: 217 Rating:
|
Hi! You can use the 'IE General' from the Hardware Catalog (from SIMATIC PC Station -> CP Industrial Ethernet -> IE General -> 'Your installed SOFTNET S7 Version, e.g. V6.2 SP1'). But you are not able to use 'IE General' on the 'IF1-4' slots of the WinAC RTX. On these slots you can only use a CP 5611 or CP 5613. A good example for Etherne communication with WinAC RTX can be found here: S7-Communication with WinAC RTX and S7-300 via Industrial Ethernet |
|
Greetings, Chris |
|
Follow us on