2/21/2007 9:32 PM | |
Posts: 5 Rating:
|
Please I need urgent help. When trying to start simovert VC 6SE7033 DC to AC the unit does not start. On the PMU only appears E. The PMU does not work at all. |
2/23/2007 10:16 AM | |
Joined: 10/11/2006 Last visit: 8/29/2025 Posts: 6037 Rating:
|
Hello Biser, did you try to start up the drive without any cable connected to the serial interface? If there is a earth connection on pin 4 of the serial interface, the drive goes to the boot mode and shows "E" at PMU. Attached find a boot describtion, where the serial cable is described. (It is for MASTERDRIVES MC, but the cable, as shown on page 8, is the same.) Best regards TechTeam AttachmentREADMEMC.pdf (699 Downloads) |
With best regards, |
|
Follow us on