(0)| 4/16/2012 7:07 AM | |
|
Posts: 108 Rating:
|
Hi, I am having problems setting up a connection between an IM151-8PN/DP PLC and a PC station with a WinCC professional runtime module. I would like to be able to access the PLC variables from WinCC directly, without having to create HMI tags in WinCC and link these to memory areas in the PLC. Is this possible? I have seen that there is a problem creating an HMI connection using the network view of the "Devices and networks" window, and have tried following the instructions given in entry ID 58112141, but this did not work either. Any help would be much appreciated. Thanks Jason |
| 4/16/2012 2:02 PM | |
|
Posts: 3037 Rating:
|
Hello, here you can see in the following link how you can use plc tags. How do you migrate tags from STEP 7 V11 to WinCC V11? Tweety |
| 4/17/2012 3:00 PM | |
|
Posts: 3037 Rating:
|
Hello, Yes, this is right. You can not use this FAQ with WinCC Professional and IM 151-8 How do you migrate tags from STEP 7 V11 to WinCC V11? You can not copy the tags from plc to WinCC.You must create the tags in the tag table editor of WinCC new. You can use the settings of the following FAQ. Why is the graphic configuration of a connection to an IM151-8PN/DP CPU not supported in WinCC Professional? If the connection to the plc does not work, you check the access point in the PC/PG settings.Tweety |
| 4/18/2012 5:29 AM | |
|
Joined: 10/7/2005 Last visit: 12/29/2025 Posts: 3052 Rating:
|
Hello jasonr An"Ethernet address" is the "MAC address"andalso known as"Ethernet hardware address" or"Hardware address" or even referred to as "Physical address", just to keep everyone on their toes (see also http://en.wikipedia.org/wiki/MAC_addressfor more). Anyhow, every Ethernet device has a unique "six two-digit hexadecimal" based MAC address (well, should have) and you'll find it imprinted on your IM151-8. This MAC address is what you are meant to use and I hope thishelps (and also hope that Siemens will fix up the issue with the IM151-8 linkage to WinCC advanced). |
|
Cheers |
|
| 4/18/2012 5:33 AM | |
|
Posts: 108 Rating:
|
Ah, ok. So will I be able to run a simulation with an IM151-8 PN/DP CPU connected to a PC station running WinCC professional runtime? Jason |
Follow us on