3/27/2007 11:21 AM | |
Posts: 23 Rating:
|
Hi, I have a small project as follow : i want to connect the Micormaster420 with the PLC CPU 315-2DP via Profibus. I connected the MM and the PLC successfully, and read / write some parameters via PKW. But i can't monitor the PZD. Someone who has experience please tell me how to config the MM420 to solve this problem, how to on/off the drive and change the speed of the motor? Thanks! This is my project. AttachmentTestProfiMM4.zip (677 Downloads) |
3/27/2007 4:09 PM | |
Posts: 2 Rating:
|
Hello, I am going to use the attached file ifI ever get my drives to accept the PB board. Hope it is of some help to you. Steve AttachmentMm4_prof.zip (706 Downloads) |
Follow us on