(0)| 8/23/2012 6:16 PM | |
|
Posts: 4 Rating:
|
hi all, First of all verry nice forum,i really learned mutch down here. But now my first problem. I'm working on a program and i want to have a log so that i can see when an outlet was high. I've put a message every time the pulse goes high with a timedate so that i can see what the date and hours were when the outlet was on. the question is if i can put the message in the bachground and only show them when i want without setting the hour otherwise? and is there a more simple way to switch on every message with a pulse? I hope my question is a little understandable, and thanks for the help already.. I made a fast example of the way i see it now to write.. Attachmenttest log.zip (348 Downloads) |
Follow us on