(0)| 2/25/2013 7:22 AM | |
|
Posts: 2 Rating:
|
Good day, colleagues. I want to know, if it's possible (and how) to connect sinamics DCM with comfort panel via profibus. Sinamics DCM config: Advanced-CUD FW version: 1.3.0.2; CBE20. I can establish a direct connection between Sinamics DCM and TP700 comfort panel via Profinet by CBE20, but when I try to do that via Profibus DP by onboard control unit I do not get any results. Although, related connectors have following values: r963 "Profibus baud rate": [3] 187.5 kbit/s r2054 "Profibus status": [2] Connection OK (baud rate found) I thought that deal is in CBE20, but after I configured parameter 8839 like this: p8839[0] "Interface 1": [1] Control unit onboard p8839[0] "Interface 2": [0] Inactive there was not result again. In the attachment I'll put project for HMI TP700 comfort, in which i try to get just a status word from sinamics DCM (e.g. P899). If possibilities to communicate sinamics DCM with Comfort panel by Profibus exist, could you give me a step by step guide to configure HMI via TIA portal, and a list of parameters for sinamics DCM. Is that possible to establish Profibus connection with other simatic panels (for example basic type)? Thanks in advance!!! AttachmentKVSD_HMI.ZIP (448 Downloads) |
Last edited by: Dmitriy2030 at: 2/26/2013 11:58 AM |
|
Follow us on