3/30/2013 7:19 AM | |
Posts: 1 Rating:
|
Iam trying to read alarms and measurands from Siemens Relay 7SR11 as per Data communication table for IEC103. So far I am successful in connecting to relay and reading some values ,however all values are not getting updated for eg V, P, Q,F . Please help me . find the setting I am using for reading measurands. function 183 info no 148 func type 9 position 1-9 ( position was assumed by me as manual doesnt say anything about it but ABB RTU config has a field for it) by using this config I can read values of I1 , I2 and I3 only ie Position 1,2,3.
Attachment7SR11 and 7SR12 IEC103.pdf (434 Downloads) |
Follow us on