(0)| 1/4/2011 1:39 PM | |
|
Posts: 8 Rating:
|
Hello. IfIdo the "Optimization of closed-loop field-current control" (P50051=24), I get the fault F60050 with the code 101 (Alpha G limit reached when determining the Rf), and the remedy suggested is: "Check field circuit for interruption (e.g. due to blown fuse)". I check the field circuit, and it is OK. And if I connect the drive, the field current reaches the nominal current (17A). The field circuit seems to be OK because this motor operates normally with an old Eurotherm DC Converter control module, and we don´t have any problem.
If the field circuit is ok, why do I get this fault? How can I complete the "Optimization of closed-loop field-current control" correctly? Info: AttachmentSINAMICS DCM.zip (667 Downloads) |
Last edited by: Mr Mata at: 1/10/2011 5:39 PM |
|
Follow us on