6/26/2013 8:01 AM | |
Posts: 49 Rating:
|
Hello Expert, I am working on a project based on cpu 315 2 pn/dp & communication with simocode prov, I required more than 10 bytes data from simocode so i used sfc59 for read data.Now problem is that where i can find the RECNUM(in simocode).here i attach the screen shoot of the sfc 59 instruction. Thanks & Warm Regards Attachmentuntitled.zip (223 Downloads) |
6/26/2013 9:49 AM | |
Joined: 10/7/2005 Last visit: 9/14/2025 Posts: 3049 Rating:
|
Hello rabi you use the number of the Data Record that you want to read from the SIMOCODE as the value for SFC59's "RECNUM" parameter. SIMOCODE's have a fair few Data records that you can read (and/or write too), have a look atAppendix B fo the System Manual SIMOCODE pro which contains all the detailsfor each one. I hope this helps |
Cheers |
|
Follow us on