6/28/2013 6:03 AM | |
Posts: 262 Rating:
|
Hi, Like to add one more thing... the MCCB which has been recommended in Type 2 chart of siemens is Starter Protection MCCBs which has only SC protection and hence best suitable with Overload realy and contactor combination. MPCB have characteristics are similar to what sq. cage induction motors are required and hence these combinations have been recommended. One more thing.. Siemens provides all test reports for Type2 co-ordination combination from Neutral Test Laboratories. Attaching all the possible combination of TYPE 2 with MPCB or with Fuses herewith AttachmentComplete Type 2.pdf (949 Downloads) |
Follow us on