12/24/2013 2:36 PM | |
Posts: 11 Rating:
|
Hi, There is an optionalNVIDIA QUADRO NVS 295 for rack PCs (e.g. IPC647C) but it is not available for Box PCs (e.g. IPC627C). Why is that? I also readthiswhite paper from Siemens regarding Graphics in IPCs, and I understood that one should be careful with adding graphic cards to non-rack IPCs since their power supplys might not take an external graphic card. Has anyone tried the NVIDIA QUADRO NVS 295 (or any other card) with Box IPC, or knows that it works or doesn't work? Thanks, Sinan. |
Last edited by: Sinan! at: 12/24/2013 2:37 PM |
|
1/7/2014 2:52 PM | |
Joined: 10/18/2012 Last visit: 8/22/2025 Posts: 225 Rating:
|
Hello Sinan, I didn't try this graphics card in that IPC.But according to the Operating instructions of SIMATIC IPC627C, chapter Technical data > Current/power requirements of the devicein table "Typical Power values" the maximum Power consumption of a PCI-/PCIexpress expansion card is mentioned with 37 W. Nvidia states the maximum power consumption of it's the QUADRO NVS 295 on it's specifications page as 23 W. So from this point of view it should work perfectly together. Please let us know if you are successfull with this setup! regards, xnor. |
Follow us on