3/20/2014 11:51 PM | |
Posts: 15 Rating:
|
When the equipment is running a general fault will stop it , i am operating via profibus to PLC and SCADA . What could be the cause ? Look in my attached file its a SIMOCODE DP.
AttachmentPUMP 103.zip (465 Downloads) |
Last edited by: MacMbi at: 3/26/2014 7:30 PMLast edited by: GrasserF at: 3/21/2014 12:04 AMnew subject after splitting from /tf/WW/en/Posts/77411#top Last edited by: 2312 at: 3/20/2014 11:55 PMt also does happen to PRO V |
|
3/21/2014 9:56 AM | |
Posts: 467 Rating:
|
hello 2312, This problem can unfortunately not be answered without further information .Urgently needed is :- The detailled error message (=> please connect in case of General Fault with PC-Software Win-Simocode and read out the detailled error message via Target System -> Control / Signal)- The wiring diagram of the motor feeder I propose to contact our Technical Assistance mailto:technical-assistance@siemens.com kind regards LesPaul |
Follow us on