(2)| 5/28/2014 12:29 AM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
HelloLucky123, *** Blue Moderator: First part was deleted. It is included in the original thread WINCC Flex, VS WINCC Classic vs, WINCC Advanced vs WINCC Professional. *** 2-
64K tags license is only available in WinCC TIA Professional and SIMATIC WinCC "Classis" as you call it. Both supports working in excel. Take care of the following: 1- At this 64K power tags, you might need to consider server client configuration. 2- You might also need to check total number of connections you have and maybe you will need more than a server/OS. 3- I also can't correlate the 64K tags to only 50 screens. Anyhow, you can find all information regarding performance, configuration, licenses and part numbers in thecatalog. Best regards, H-H |
Last edited by: Blue Moderator at: 5/30/2014 10:23 AM |
|
This contribution was helpful to
|
|
| 5/30/2014 6:32 PM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
HelloLucky123,
To be honest wih you. I didn't understand your application and your display tree. Anyhow, Both can handle 200 screens. I just recommend to study technical specifications for both software in the above mentioned catalog.
list prices are almost the same. No big difference. However, you should check the actual price in your country because I believe both don't have the same discount factor. Only your local Siemens office can tell you which one is cheaper. Now we come to a good point. For S7-300 you can either use TIA or SIMATIC Manager for PLC software development. For S7-400H you don't have a chance with the TIA and you have to go for SIMATIC Manager. Now when it comes to HMI software, both can handle S7connections with S7-300 and S7-Fault tolerant connection with H stations. Both have different Redconnect licenses. TIA WinCC SIMATIC WinCC Another point, 1- Integrating WinCC in SIMATIC Manager is guaranteed 100%. 2- AlthoughSiemens released a proxy server to integrated a STEP7 project with TIA WinCC, you still need to contact Siemens support to make sure that the device proxy will work with named connections of S7-400H. Best regards, H-H
|
| 5/30/2014 6:39 PM | |
|
Joined: 6/8/2013 Last visit: 12/15/2025 Posts: 160 Rating:
|
Dear, You use SCADA wincc 7.2, it is latest scada software and more reliable so easy to use.
|
Follow us on