9/5/2007 7:59 AM | |
Posts: 3149 Rating:
|
Hi perhaps you can use a different configuration as mentioned in this application http://support.automation.siemens.com/WW/view/en/24023824 nemo |
9/5/2007 11:32 PM | |
Posts: 25 Rating:
|
Jim, The requested files are attached. Thanks for taking a look. Nick Attachmentbytcatengstat hw.zip (469 Downloads) |
9/6/2007 9:54 PM | |
Posts: 25 Rating:
|
Jim, Thanks for the support on this one. I'm thinking it's some kind of simple configuration issue, and I appreciate any input that you might have. I experted the Netpro connections again, with the connections checkbox checked. These are in the attached file. The controller is an APACS+, I am simulating the system using the 4mation simulator, but I don't think I can add the connection to Netpro. I am getting data transfers between the ES/OS Server WinCC app and the 4mation simulator on the same machine without any problems. I checked the Server Data on all three PCs, and they all point back to the ES/OS Server. However, all three PCs also say 'No preferred' under the preferred server column. I also checked the Graphics Runtime tab on the Computer properties, and all three PCs are pointing back to their respective projects on the ES/OS Server. I regenerated the server data, and downloaded to the client PCs, with no improvement. We are using internal NICs, and not CP-1613-A2s. I double checked that in the configuration. I have tried ISO instead of TCP/IP, with no improvement. If you have any ideas, I would like to hear them. Thanks, Nick AttachmentBYTCATENGSTAT net.zip (505 Downloads) |
Follow us on