10/17/2014 2:35 PM | |
Posts: 467 Rating:
|
hello, The maximum Measuring range of the requested relay 3UG4622 is 10A!!!With AC currents I > 10 A it is possible to use 4NC current transformers as an accessory, see Catalog LV 10 "Low-Voltage Power Distribution and Electrical Installation Technology".Here the link: http://w3app.siemens.com/mcms/infocenter/content/en/Pages/order_form.aspx?nodeKey=key_9177913&infotype=catalogs&linkit=null |
11/10/2014 12:30 PM | |
Posts: 467 Rating:
|
hello, The chosen 3UG432 relay is connected like a normal voltmeter (between two phases), so the current is not relevant! kind regards LesPaul |
Follow us on