(0)| 11/22/2007 6:33 PM | |
|
Posts: 3 Rating:
|
Thanks for the help, but I can not move off the fault to change any prams. and p070was 25. when I started |
| 11/23/2007 3:50 PM | |
|
Posts: 3 Rating:
|
Just checked out the cable it's okay.I was on line with one drive, downloded the file the OEM sold me and had no luck with running. 701 would not change to 460 volt from 240, and a lot of the paremeters lit up red and did not match the drive so I reset the drive to default using the PMU. the only thing I may have screwed up was 366 I used 0 and now I can not do a thing but look at f035. I am sending to files. The one we bought and one I made from printed notes in the binder that came with the machine. Thanks forthe help AttachmentOEM file.zip (620 Downloads) |
Last edited by: chawk at: 23.11.2007 22:39 |
|
Follow us on