4/27/2015 4:07 AM | |
Joined: 9/27/2006 Last visit: 9/18/2025 Posts: 12413 Rating:
|
Hello opauto; This would be a limitation of PPO3, a profile type defined by the Profidrive Standard. See the images in the following link to see the differences between the different PPOx: https://support.industry.siemens.com/cs/document/8894363?lc=en-US The section of the PPOx that interests you is the PZD (process data). PPO3 only has the 2 basis PZD words, the Control Word ansd the Speed Reference. PPO5 adds 8 more PZD words, PPO4 and PPO2 add 4 PSD words each, so you could insert the current consumption if it is an available parameter from your model of drive. You will have to look up the Operating Instructions for your specific drive to locate the parameter number (do a search in the Search box above), and find out how to integrate it inside the PZD area for Profibus comms. Hope this helps, Daniel Chartier |
Follow us on