4/11/2015 7:38 AM | |
Posts: 4 Rating:
|
Dear sir,
Please tell us how to see this parameter.
|
4/11/2015 10:30 AM | |
Joined: 3/28/2015 Last visit: 9/14/2025 Posts: 725 Rating:
|
What is the setting of P0003? P0003 Defines user access level to parameter sets. The default setting (standard) is sufficient for most simple applications. Possible Settings: 0 User defined parameter list - see P0013 for details on use 1 Standard: Allows access into most frequently used parameters. 2 Extended: Allows extended access e.g. to inverter I/O functions. 3 Expert: For expert use only. 4 Service: Only for use by authorized service personal - password protected. P0004 Filters available parameters according to functionality to enable a more focussed approach to commissioning. Possible Settings: 0 All parameters 2 Inverter 3 Motor 4 Speed sensor 5 Technol. application / units 7 Commands, binary I/O 8 ADC and DAC 10 Setpoint channel / RFG 12 Drive features 13 Motor control 20 Communication 21 Alarms / warnings / monitoring 22 Technology controller (e.g. PID) |
Eng.Mohamed Ibrahim |
|
4/15/2015 10:15 AM | |
Posts: 4 Rating:
|
yes , also try it and also i have also try without profibus unit for parameter setting. Please do the needful. |
4/15/2015 12:04 PM | |
Posts: 30 Rating:
|
Hello kk1986, you can try "Reset Factory", then you will see P0004. (stored all parameter before do this :) ) |
4/15/2015 12:55 PM | |
Posts: 4 Rating:
|
could u explain how do it without seen P970 |
4/29/2015 8:32 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Confirm your drive part number friend |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on