(2)| 11/27/2007 10:40 AM | |
|
Posts: 1776 Rating:
|
Hi, for channel driver see the following link, cause, as i know the S5 channels are not more included in WinCC http://www.industry.siemens.com/IT4Industry/EN/SOLUTION_SERVICES/SIMATIC_ADDONS/KANAL.HTM |
| 12/14/2007 4:26 PM | |
|
Posts: 22 Rating:
|
Thanks for your help. I ordered the CP1613, waitng for its coming. But I have already questions. In the link below, it is written that we don't need to change Plc program, when we use PMC S5 Ethernet channels. http://www.industry.siemens.com/IT4Industry/EN/SOLUTION_SERVICES/SIMATIC_ADDONS/KANAL.HTM I've made research about PMC and understand that a PMC - WinCC communication is done with Send/Receive Interface and PMC blocks. Our system is working well with OP47 (Plc program don't have any problems i mean). But we'll use WinCC V6.0 instead of Op47. My question is: Will I make changes in the PLC program? Will I make any configuration at PMC Handling blocks? (FB205, FB206, FB207...) Best regards |
| 12/15/2007 8:08 AM | |
|
Posts: 22 Rating:
|
Hallo J_Bell Thanks for giving answer. Yes I want to replace OP47 with a PC with WinCC. I know that my communication with PLC and Coros is using PMC communication. Because I send my Coros's *.s5l file toan expert in the hmi support department and he said me that the using communication is PMC. I also export my S5 programs Assigment list. There are PMC blocks called int S5 program.Now I'msure it is using PMC(I attached the assigment list and my systemsschematicyou can check it in the system.zip) Yes the easiest way is to use the same communication until now. About the CP1613: Our CP1430 TF card uses SinecH1 network (with PMC). It connected to the OP47 with an CP1413 card. We need to use the same card. But this card is too old and hard to find. Expert said that we can use Cp1613 instead of Cp1413. Now my question is same. Will I make any change in the Plc programing, especially in the PMC Handling channels? Thanks in advanced. Best regards DerJunge Attachmentsystem.zip (649 Downloads) |
| 12/17/2007 7:36 AM | |
|
Posts: 22 Rating:
|
Thank you very much J_Bell You've helped me too much. Now, I'm waiting for the card. Then I'll tell the result here Thanks alot DerJunge |
Follow us on