(0)| 5/26/2015 8:13 PM | |
|
Posts: 4 Rating:
|
Hi, Dear All, I have a 6RA70 application with T400. I am trying to download the user program but during the compilation an error message appears with the follow information E-SDE-LD exits with errors. Details see file c> temp\psw.mp3 I have opened the file above and found some information about violation or something on sde-gcc.exe In order to solve this problem, I have some questions. 1) May I download the user program with that error 2) Is there a hotfix for D7-sys. According to the message 1330, this is a D7-sys internal error 3) What cause that problem. System Settings STEP 7 v 5.3 OS- Windows XP Professional SP3 Attached the screen and psw. mp3 AttachmentFile.zip (337 Downloads) |
| 5/27/2015 5:56 AM | |
|
Joined: 8/25/2006 Last visit: 12/30/2025 Posts: 2221 Rating:
|
Hello. 1. No, you can't download with any errors. Compilation must be error-free. 2. Which version of D7-SYS you have? All available SP and HF you can find here. 3. I think there is something wrong with SW installation. Try to reinstall at least D7-SYS or install HF or SP for D7-SYS if available. |
| 5/27/2015 8:20 PM | |
|
Posts: 4 Rating:
|
The version is correct. I am using two user libraries on my project fba121 and fbabas. Because of these libraries it was necessary using TDC |
Follow us on