10/6/2010 11:30 PM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi, you don't mention if you are using a USB-RS232 converter which is where 95% of people struggle. Make sure you have selected the correct port number in the interface tab of Drivemonitor's "ONLINE settings" menu. You can determine the relevantport that is being used bythe Control panel and by looking into the system hardware settings. Otherwise, also check P2013 = 127 (Variable word length) Other considerations may be that the panel/or cable is defective, also,can you try this on another laptop with a serial port? Other useful links: http://support.automation.siemens.com/WW/view/en/24072800 /tf/WW/en/Posts/46826 Cheers, Graeme |
1/13/2011 2:28 AM | |
Joined: 10/17/2007 Last visit: 9/15/2025 Posts: 4452 Rating:
|
I meet same problem, see link blew: Siemens expert,please help us tosettle this problem. 1st post: /tf/WW/en/Posts/52053#top 2nd post: /tf/WW/en/Posts/52369#top thanks. |
Last edited by: nulizhang at: 1/15/2011 3:47 AMmodif. spelling err Last edited by: nulizhang at: 1/13/2011 2:30 AMadd 2nd post link. If you like my comments please |
|
6/15/2015 3:12 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
|
Follow us on