7/22/2015 7:01 AM | |
Joined: 8/25/2006 Last visit: 9/10/2025 Posts: 2218 Rating:
|
Hello. Look for description of K0009 at the manual, chapter 9.1: K0009 is assigned to different signal quantities. Which signal quantity it actually refers to is dependent on the selector switch (parameter) at which connector number 9 is set. A description can be found under the relevant parameter number in the Parameter List. If the Parameter List or block diagram does not contain any reference to a special function in relation to selection of connector K0009, then the selector switch (parameter) concerned must not be set to "9". This means that you should find the parameter which have value of K0009 in the function diagrams and read the description at this sheet, e.g. look at sheets G160, G161, parameters P606, P604. If these parameters are set to K0009, this means their values are negative signal from P605, P603. |
7/22/2015 9:02 AM | |
Joined: 7/11/2015 Last visit: 4/14/2025 Posts: 6 Rating:
|
Good day! The issue is not the topic, but... AttachmentJP0.rar (331 Downloads) |
Last edited by: DIMA_FDA_STD at: 7/22/2015 9:05:57 AMLast edited by: DIMA_FDA_STD at: 7/22/2015 9:06:27 AM |
|
Follow us on