6/28/2015 11:36 AM | |
Posts: 1 Rating:
|
sir, I having the error F 0022 on micromaster 440(6SL3351-1AE32-6AA1) I checked the motor ok |
6/28/2015 11:43 AM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
I found in German Forum this from User fichtel:
https://support.industry.siemens.com/tf/ww/de/posts/fehler-f0022-an-mm420/8572/?page=0&pageSize=10 |
8/20/2015 12:21 PM | |
Posts: 112 Rating:
|
Iam using MM440 5.5kW. it works very well. but when the drive vibrates it gives F0022. what should I do? thanks Adi |
8/21/2015 3:26 PM | |
Posts: 112 Rating:
|
ok thanks. i will examine all internal connectors can see. |
This contribution was helpful to
1 thankful Users |
Follow us on