10/23/2012 7:33 PM | |
Posts: 2 Rating:
|
I am trying to replace a Micromaster 3 Vector that was destroyed/shorted with a MM440. The machine is quite old and unfortunately the documentation for the Vector drive is limited to this one page which I have attached. The drive was configured to run with a reset tied to DIN1 which I have setup as a fault acknowledgement via P0701 and that seems to work fine. DIN2 is set to run in forward mode and from what I am told it used to run the motor at 15Hz. DIN5 was used as the reverse run condition also at 15Hz. If I understand the ladder correctly (poor commenting) I think this will never turn on with the forward condtion so it would be a separate run state just reversed direction. DIN4 is used as a high speed enable. If the motor is running in either forward or reverse and this is selected, it will increase output frequency set point to 25Hz. I am not sure how to set the parameters to allow this operation. I specifically need help with the 701-705 and 1000-1006 parameters and then any parameter which may be affected by those. Any help/advice will be greatly appreciated. Thanks, John
Attachmentmachine print.pdf (447 Downloads) |
Follow us on