7/15/2016 1:01 PM | |
Joined: 12/9/2010 Last visit: 5/27/2025 Posts: 165 Rating:
|
Hi Siwarexi, That would be great and very appreciated. I couldn't attach the project since it is to big but I've provided a link where i uploaded it. The size of the project is 17mb, I don't know how to get it smaller to attach it directly to the forum. http://speedy.sh/SHQJH/rQx-WP241.zip I guess the networks that you need to look at is Network1 in cyclic interrupt OB30, this network contains the CMD_Handling block for two WP241. Network1 in main OB, this network contains the WP241 adressing. Network14 contains the code to control the WP241 with commands to CMD2. (This is working but not for command 2005, but since it doesn't work with CMD_handling either I think that this network is OK) |
Last edited by: rQx at: 7/15/2016 1:01:32 PM |
|
Follow us on