4/8/2008 4:28 PM | |
Posts: 2661 Rating:
|
Did you check your Picture Tree? |
4/9/2008 7:43 AM | |
Posts: 12 Rating:
|
Yes, I checked the Picture Tree. It's ok. Also preview in the OS Project Editor shows the Push button generated. |
4/9/2008 4:48 PM | |
Posts: 2661 Rating:
|
Try the WinCC runtime after runningthe OS Project Editor with settings as shown in the attachment. AttachmentOS_ProjEditor.pdf (597 Downloads) |
4/10/2008 7:52 AM | |
Posts: 12 Rating:
|
These four items were not ticked off. However, when I ticked the items off, nothing was happend. Also I forgot to mention that in the upper part of the overview area there's a message "not active". I use PCS7 v6.1. I attached zip file in which two files are included(overvew and runtime). Thank you for your help. Cebona Attachmentpict.zip (377 Downloads) |
Follow us on