(1)| 10/13/2016 10:09 AM | |
|
Joined: 6/30/2014 Last visit: 1/6/2026 Posts: 476 Rating:
|
Dear COMOS admins and users, ==> as you may know, you can find the official Documentation for COMOS accessing it from COMOS itself, or over the file explorer, as it gets copied on your PC/Notebook with it's installation. ==> But it could happen that you may prefer to have the COMOS documentation in PDF files. Of course Siemens offers that too, here you see the internet site, where you can download a Dockupack, which contains the whole documentation in PDF format. Please see my screenshot attached here, to see where to click... very easy. At best, please click on the link here above to get on that homepage. You will get a zip file, so unzip it as soon the download is done. In the list of the PDF files, you will also find the file named "COMOS_Help_EN.pdx": this is the best address to search the whole documents (without having to open them manually) with a particular keyword. On the other hand, if you are looking for the documentation (i.e.) about "COMOS License Management (COMOS LM)" and you know that you can find it in the PDF file named "COMOS_Platform_Administration_enUS.pdf", feel free to open that particular PDF file. As well, you can always press ctrl and f to use the search function in a PDF file, to enter the keyword your are searching for. If you like, try ctrl and l too, to read a particular manual in full screen mode. ==> If you do not need the whole documentation in PDF files, but only one document as a PDF file, you can download that/one particular file from the same homepage, just scroll a bit down to find it there. Just in case you saw other interesting scenarios, please share those with us all. Enjoy it, have a great day, SuperPippo |
Last edited by: SuperPippo at: 10/13/2016 10:12:45 AM |
|
Follow us on