(0)| 5/11/2008 11:07 AM | |||
|
Joined: 9/27/2006 Last visit: 12/26/2025 Posts: 12474 Rating:
|
Hello tt_singh; I believe you are lloking for S7 F-Configuration PackThis is a component of the optional package S7 Distributed Safety: The S7 Distributed Safety optional package has two components as follows: • "S7 F Configuration Pack V 5.3 SP2" • "S7 Distributed Safety Programming V 5.3"
First, this is not a free downloadable package. You must enquire for purchase detailsfrom your Siemens rep. Second, this CPU is a SafetyPLC (F-CPU), probably including F-IO modules (recognizable on their yellow bezel), and including a Safety Program. This program is not accessible through standard Step 7 utilities; it uses specific F-libraries (included in the S7 F-configuration pack), it is compiled apart from the non-safety program, and is subject to an acceptance test (done by the Distributed Safety software).So you should read up on the DistributedSafety programs before you attempt to modify it. Now, for more details on the S7 F-Configuration pack specifically, this ishow Siemens describes what it does: S7 F Systems optional package This documentation describes S7 F Systems. S7 F Systems is the configuration and programming software for S7 F/FH Systems. With S7 F Systems, you receive the following: ● Support for configuring the F-I/O in STEP 7 with HW Config ● Support for creating the safety program and integrating fault detection functions into the safety program ●F-Library containing F-Blocks that you can use in your safety program ● Moreover, S7 F Systems offers functions for comparing safety programs and for assisting you with the system acceptance test. ● Support for operating fail-safe parameters of a PCS 7 OS during operation (Safety Data Write). |
||
Last edited by: dchartier at: 5/11/2008 11:14 AMLast edited by: dchartier at: 5/11/2008 11:11 AM |
|||
| 5/11/2008 1:38 PM | |
|
Posts: 56 Rating:
|
can you give me the above mentioned softwre S7F configuratio and distribution safety.Please send me on this e-mail if possible k.tiwana@gawab.com |
Last edited by: tt singh at: 5/11/2008 1:45 PM |
|
Follow us on