2/20/2017 11:41 AM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Hi Techalone, here are some general information about Masterdrives: The link to the compendium Masterdrives VC 3.4:http://support.automation.siemens.com/WW/view/en/13472409 The link to the commissioning tool DriveMonitor:http://support.automation.siemens.com/WW/view/en/11769381 With p445 the incoming set point via p443=3002 (from Profibus) can be scaled between -200 .... +200%. I recommend strictly contacting the manufacturer before changing anything in the system |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on