3/1/2006 7:54 AM | |
Posts: 3149 Rating:
|
Hi , there´s a little, cute tool: http://support.automation.siemens.com/WW/view/en/9985721 nemo |
3/1/2006 9:43 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
You can also use the GetHWDiag function in WinCC to open the PLC's Diagnostic Buffer. I have attached an FAQ detailing how to do this. There is a Dynamic Wizard that drill you into the PLC code. This wizard creates a script that can then easily be adapted to call up the diagnostic buffer instead of the PLC code. I hope this is of use. Salma AttachmentWinCC Information Pages.zip (1221 Downloads) |
Follow us on