5/27/2008 11:28 AM | |
Posts: 13 Rating:
|
Dear diwa thanks lot for replay but i have also problem F008 in some drives fault accure afeter hours pls tell me about this thanks sm rana |
5/31/2008 11:37 AM | |
Posts: 13 Rating:
|
Dear Mr Diwa thanks to you i will try this SM rana |
5/4/2017 4:23 PM | |
Posts: 2 Rating:
|
DEAR. Para la solución de la alarma F06. Se cambio el encoder que esta acoplado al eje del motor del inversor instalado en el bus DC. Este ocasiona, que se interprete como una detención del motor por lo que ocasiona que el equipo regenere. No existían alarmas en los equipos re-generativos. Solo alarmas en los equipos inversores. ------------------------------------------------------------------------------------- DEAR.
The encoder that is coupled to the motor axis of the inverter installed on the DC bus is changed. This causes it to be interpreted as an engine stoppage causing the equipment to regenerate.
Only alarms in the inverter equipment. AttachmentSolucion F06 Siemens.doc (546 Downloads) |
Last edited by: Min_Moderator at: 5/5/2017 2:24:34 PMTranslation |
|
Follow us on