5/5/2017 9:46 PM | |
Joined: 5/6/2010 Last visit: 8/28/2025 Posts: 90 Rating:
|
I had this problem noted here: Where I could no longer open my project in the drive software via Simatic Manager. I had not used that Windows 7 laptop for STARTER for several years and at some point IT must've upgraded me to 64 bit office. I was not going to remove office and re-install. I found this on the internet: http://gamblisfx.com/how-to-install-ms-access-database-driver-32-bit-and-64-bit-on-a-single-machine/ You use the same link as the on at the bottom of the Siemens link but you run the executable with "/passive" at the end via the DOS cmd window. This worked for me and MS office still functions properly. Error messages: The project is write-protected or is already being used by another process on a different computer. Error occurred while opening the project. Access to the project has been denied. |
Follow us on