9/5/2017 2:37 PM | |
Posts: 2 Rating:
|
I have an application that needs a, preferably mini PCIe card, GPS receiver. Nominally, the MEN Mikro PX1 and the Connect Tech Mini PCIe GPS cards are suitable. Apparently, they do not require a specific driver. The USB2UART interface is supported under Linux, kernels higher than 3.0. Is the Kernel used in Yocto appropriate? If not does anybody know of alternatives, apart from a smart phone? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 9/5/2017 3:34:28 PMNew subject after splitting |
|
Follow us on