7/8/2008 3:42 PM | |
Joined: 3/29/2006 Last visit: 5/29/2017 Posts: 151 Rating:
|
The drives in your HW Config are from Step7 standard-catalog via GSD-files; see attachment "MD_Standardfunktionalitaet.doc" . To select drives with DriveES interface, you must install DriveES Basic on your computer; see attachment "DriveES-Profile.doc". IfDriveES Basic is installed on your computer, you can delete the gsd-objectes and replace it by the DriveES-objects with the same telegramm. If you have a Step7-project with DriveES-objectsand you want to open it on another computer, DriveES Basic MUST be installed on that computer, too. http://support.automation.siemens.com/WW/view/en/27726644 Only with DriveES-objects it is possible, to have access to the drives with DriveMonitor via DP. DriveMonitor communication via USS must be possible. Check parameter P700 to P703. AttachmentCBP_CBP2.zip (356 Downloads) |
7/15/2008 3:04 PM | |
Joined: 3/29/2006 Last visit: 5/29/2017 Posts: 151 Rating:
|
Your screen-shot of hardware-catalogue looks good !
6SE7033-2EG50-Z is Motioncontrol (Firmware V1.x ) This is the setting to go online via COMx and serial interface X300 on the drive
AttachmentMasterdrives on DP.zip (361 Downloads) |
Follow us on