4/10/2017 12:36 PM | |
Posts: 48 Rating:
|
Hello , could you please inform me how can I connect my Laptop to a simoreg dc master 6RA70 to look the program inside T400 ? thanks . |
4/11/2017 6:21 AM | |
Joined: 8/25/2006 Last visit: 9/15/2025 Posts: 2218 Rating:
|
Hello. What order number of your T400?
If your T400 is the first one, then you can download to it CFC-program via RS232-cable. Look at this manual, chapter 5.4. Uploading of CFC-program is not possible. If your T400 is with standard program you can download/upload only parameters backup using DriveMonitor with the same cable as used for connection to the drive (X300 in Simoreg).
|
This contribution was helpful to
1 thankful Users |
4/11/2017 10:16 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, DriveMonitor is useful tool to excahnge parameters between drive & PC. For 6RA70 user do not have any software tool which can access drive programe directly. Please refer attached file for more details. Attachment6RA70 DriveMonitor Description .pdf (687 Downloads) |
12/15/2017 12:33 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by Mubashir Jalil is split to a separate thread with the subject RPM's of SIMOREG 6RA70 DC vary a lot. Best regards |
Follow us on