12/1/2014 2:04 PM | |
Posts: 6 Rating:
|
Hello I try to install WinAC RTX 2010 on PC with OS Windows 7 Professional 32bit - no virtual machine. I have a big problem with that. From the SW package the installation wizard is able to install only RTX 2009. After that, each installation of another sw of this package (Automatic Licence Manager, Windows Logic Controller, WinAC Time Sync) finished with the dialog window for restarting system. But after restart nothing another is installed. Look at the attached screens. I tried also install RTX as the first SW on the windows (before anothe SW package) - the behaviour is the same Can you give me some advice ? Note: the attached screens are from time when there was Automatic licenced manager installed but with another package (with Wincc Flexible) - therefore there is box checked at Automatic Licence Manager in wizard of WinAC RTX 2010. Hovewer the behaviour si the same - wizard of WinAC RTX 2010 does not install another package more - it only wants to restart system AttachmentWinAC_RTX.zip (1466 Downloads) |
12/2/2014 10:57 AM | |
Joined: 11/15/2006 Last visit: 3/26/2025 Posts: 1319 Rating:
|
Please use the 2010 INCL. SP1 or even SP2 disc. |
Have Fun! |
|
12/2/2014 11:05 AM | |
Posts: 6 Rating:
|
I Tried WinAcRTX with SP1 and before installation of Win LC a got error: RTX Kernel Check Start RTX services setup error |
9/8/2015 3:43 PM | |
Posts: 1 Rating:
|
I have already this problem, How can I resolve? |
1/15/2018 1:39 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by UB_IH is split to a separate thread with the subject WinAC RTX 2010 - Nach dem Sicherheitsupdate fehlte die Verbindung zur CPU.. Best regards |
Follow us on