2/6/2018 8:50 AM | |
Joined: 1/2/2013 Last visit: 7/7/2025 Posts: 38 Rating:
|
Hi Pat, Attached please find the list of the parameters. According to your error description you might have to change some settings. Please check if the following parameters are set to the factory settings (bolt letters): 8. SPRA 9. SPRE 12: Lin 35: YA 36: YE 39: YCLS 40: YCDO 41: YCUP. If these parameters are according to the factory settings you can do a Reset (Parameter 50: PRST ALL) and try again. AttachmentA5E34928958-01en_PS2HART_FB.pdf (241 Downloads) |
Follow us on