3/15/2018 12:02 AM | |
Posts: 6 Rating:
|
Hey, I have a problem with the following combination of devices: - Siwarex U - S5-PLC - Siebert S102 - Measuring plugs in the uprights of the silo For a project that I do during my internship, I received the following problem: No values on the Siebert display of silos 1 and 2, while this still works at silos 3 and 4. It has worked for years but since a few weeks the display on the case no longer works. At other places in the factory, I do not see my values on the screen only specifically on the siebert. I have already tried the following to fix the problem: - Siwatool - Siwarex measured - The siebert is otherwise wired - New Siebert placed but nothing found there are other possibilities where it can lie See attachments Thanks in advance, Pmoess AttachmentNaamloos_bericht.zip (181 Downloads) |
Last edited by: Pmoess at: 3/15/2018 8:56:56 AMLast edited by: Jen_Moderator at: 3/15/2018 2:36:39 PMEdited text for better reading. |
|
Follow us on