8/8/2008 1:30 PM | |
Posts: 125 Rating:
|
Hi, in installation path of WinCC configure files for screen resolutions exists %Installation Path%/Siemens/WinCC/options/pdl/ for example: SIMATIC_1600x1200_S (S for Serverview) You can copy this Folder and rename in SIMATIC_1680x1050_S. Then rename and open the config file in this folder("SIMATIC_1680x1050_S.cfg") Change all entries with resolutions from 1600x1200 in 1680x1050. Change entries from 1140 in 990 and hope it will run. The new resolution is now available in Project OS Editor. More informations, see: http://support.automation.siemens.com/WW/view/en/19688107 Good luck Regards |
8/12/2008 9:21 AM | |
Posts: 55 Rating:
|
"WinCC runtime layout in wide screen monitor problem": /tf/WW/en/Posts/10352 |
Last edited by: PETER17 at: 8/12/2008 9:25 AM |
|
8/22/2008 9:13 AM | |
Posts: 40 Rating:
|
thank you very muchfor helping me with the resolution problem, it worked |
8/25/2008 6:54 PM | |
Posts: 55 Rating:
|
You are welcome Best regards PETER |
Follow us on