6/5/2018 9:50 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Could you please attach the nameplate photo of the drive? |
6/7/2018 5:55 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, I have hard copy of the manual but could not scan it. MLFB significance of 6RA2212-3AF10 is, 1 = B6C connection type (1Q), A = unit without fan i.e. natural cooling, F = 80 Amp Thyristor type TT56N. I serached & found equivalent manual (A1, A2, A3 & A5 card + parameters & fault/alarm) on Siemens web site which you can refer, SIMOREG K 6RA22; converter with mircroprocessor from 12kW to 679kW in circulating-current-free inverse-parallel (B6)A(B6)C connection or if you require specific information, please let me know so that I can try to scan specific information & attach here. HTH. |
Last edited by: Jen_Moderator at: 6/7/2018 7:28:18 AMOptimized link. |
|
Follow us on